Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
SG9101-Slide8

Displayed here is a comparison of modulation profile, center spread at ±2%. As a base or reference, no spread spectrum is shown. The most popular and default profile is the Hershey-kiss modulation profile, as the shape is similar to Hershey kiss candy. It is popular because the energy is evenly distributed across the entire spectrum. The next modulation profile is the triangle-wave, followed by the sine-wave modulation profile.

PTM פורסם ב: