Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
digital-control-slide10

The high frequency pole is also unique. Only when being used as a positive pole to compensate for low ESR zero values does it map into the s domain. When being used to act as a negative pole for phase improvement there is no mapping into the s domain.

PTM פורסם ב: