Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
digital-control-slide9

Show here is what happens when the complex zero is not at exactly the LC double pole frequency. Although the complex zero is extremely accurate, the LC components are not. A shift in either direction of 20% can result in conditional stability of the loop. So, “Keep it Real” and do not use the complex zero option except for ones own curiosity.

PTM פורסם ב: