Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
digital-control-slide2

A digital PWM control loop replaces the conventional compensation and PWM modulator used in analog with an ADC and a digital PID. Since the output from this system is a digital word, the PWM must now be a digital PWM (or DPWM). The output driver to the MOSFETs are the same as any conventional switching controller. The control loop gain and phase are determined by 4 elements, where GC is the gain of the PID known as the Compensator. The gain of the power stage shown here as Gbuck is the same as an analog implementation.

PTM פורסם ב: