Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Product List
dead-time-slide2

Inside every synchronous buck regulator is a synchronous driver which controls the two MOSFETs, turning them on and off, but also making sure that both MOSFETs are not on at the same time causing a short circuit from the input and causing things to blow up. That time period where both FETs are off is called the dead time. 

PTM פורסם ב: