Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Product List
dead-time-slide23

The non volatile memory in the XRP7704 and XRP7714 families is highly reliable and has been used in military rad hard Actel FPGAs. One should note that even if the non volatile memory has already been written, it may still be possible to change certain functions because even though a written “1” cannot be changed, a “0” can always be changed to a “1”. The new XRP7724 uses instead a YFLASH technology which can be re-written up to 100 times.

PTM פורסם ב: