Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Product List
Optical Encoder Slide 19

Compared to a mouse, an encoder is mounted on the front panel of the application. This results in a self contained assembly that does not require additional space or surfaces for a mouse pad. Compared to joysticks, encoders provide a reliable performance and functionality for mid tier cost applications. Joysticks are generally of the high volume, low cost variety (used in consumer electronics) or are very high cost precision devices used in avionics and other critical applications. Compared to potentiometers, optical encoders output digital signals that are more compatible with today’s digital devices vs. the analog output of a potentiometer.

PTM פורסם ב: