Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Product List
Optical Encoder Slide 24

The Grayhill 62C is a concentric shaft encoder. Two concentric shafts in one package allow additional functionality while conserving space and weight. Grayhill also offers the 62N, a concentric shaft encoder in which the inside shaft does not rotate but does contain the pushbutton feature. This is required when the pushbutton feature needs to be on a different shaft to prevent accidental actuation. The non turn shaft also insures that any legends printed on the knob stay in their proper orientation. Applications for these products include avionics and medical devices.

PTM פורסם ב: