Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Product List
Rotary Switches and Mechanical Encoders Slide 2

An exploded version of a Grayhill rotary switch deck section is shown here. A typical deck section consists of a common pole and it’s integral terminal, switch position terminals and a moving contact mounted to the shaft. In an actual switch, the moving contact touches, or contacts, the selected switch position terminal and the common pole. As the shaft is rotated, the moving contact is moved between the switch position terminals. Note that contact is always maintained between the moving contact and the common pole.

PTM פורסם ב: