Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Product List
Rotary Switches and Mechanical Encoders Slide 31

As the mechanical encoder shaft is rotated from one position to the next, the encoder will momentarily generate some of the other output codes before it comes to rest in the detent position of the desired output code. This is due to the fact that more than one bit is changing it’s on-off state as the shaft is rotated from one position to the next. This can be a problem in some applications. With a special output code, called gray code, or true shorting code, only one bit changes state from one switch position to the next.

PTM פורסם ב: