Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Product List
Rotary Switches and Mechanical Encoders Slide 3

The detent system of a rotary switch provides an operator with a positive indication of rotation from one switch position to the next. Without it there would be a tendency to rotate the moving contact past the desired switch position terminal. The angle of throw is the amount of shaft rotation between adjacent switch position terminals.

PTM פורסם ב: