Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
current state

It is important to remember what makes the MicroPressure sensor such a game changer. As consumers move into a more mobile world, there is increased pressure to develop smaller, lighter weight devices that can be more mobile than ever before. With calls for smaller packages and lighter weights for mobility, there is intense demand for smaller components that deliver the same results in a reduced footprint. The increased mobility also places a premium on battery life. A patient, user, or consumer can only go as far as the device’s battery will take them. Devices with power hungry components will last a fraction of the time as other devices between charges. In this miniaturized category, a lot of sensors make a variety of promises, but few of them are able to deliver in each area. For instance, many miniaturized sensors offer limited pressure options. This one-size-fits-all approach often times forces customers to alter or compromise on their designs. Most sensors in this category also do not provide a porting option. This can greatly complicate a design by forcing the design engineer to develop new ways to bring media to the sensor for monitoring purposes. Also, many sensors in the miniaturized category provide an analog-only output. While this can provide an initial lower cost, many designers lose sight of the cost of adding components for a digital conversion. If a digital signal is required, adding an A-to-D converter will greatly increase the total cost of operating the sensor.

PTM פורסם ב: