Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
spi

If the board has an SPI sensor, the designer will need six jumpers to make six connections. First, connect MOSI of J9 on the SEK002 to the MOSI on the MPR evaluation board. Next, connect SCLK of J8 on the SEK002 to the same location on the MPR breakout board. Then connect SS of T1 on the SEK002 to the SS on the MPR breakout board. Now, connect MISO of T1 on the SEK002 to MISO on the MPR breakout board. Finally, apply power by connecting the 3V3 and GND from the evaluation board to the matching headers on the SEK002.

PTM פורסם ב: