Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
Power-Factor-Slide19

Here is an application example for a CCM PFC with separate auxiliary standby power supply, as might be used in a PC supply or other consumer applications. The auxiliary supply can be implemented with a CoolSET MOSFET which is always in operation and operates off the main bus voltage. Even when the PFC isn’t running, the rectified input line will be present at capacitor C2. In standby mode, both the PFC and the PWM can be turned off. The controller supply for the PFC and the PWM supply are derived from the Auxiliary supply, operating on a common ground.

PTM פורסם ב: