Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
Power-Factor-Slide8

In Europe, the requirements are broken down into four classes of equipment, including Class A: balanced 3 phase industrial power applications, Class B: Portable Power tools, Class C: Lighting equipment And Class D: domestic equipment and motor equipment, with some distinctions in requirements based on power level. In general, equipment with an input power above 75 watts are required to meet IEC 61000-3-2-1 for harmonic content limitations. EU requirements are significant even in the United States because world wide business is most economical when equipment can be developed and sourced for multiple regions without significant changes other than language localizations. Standards such as this and ROHS have a world wide impact.

PTM פורסם ב: