Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
dc-motor-driver-slide8

The application of 3-phase brushless motors (BLDC) are the latest trend for battery-powered hand tools. The advantages over a conventional brushed DC motor are: approximately two times the power of a similarly-sized brushed DC motor; more energy efficiency resulting in longer battery life; no brushes needing to be serviced; in equivalent applications, a brushless DC powered tool is significantly lighter than a brushed motor tool; the maximum rotation speed of a brushed motor is limited by the brushes, a brushless DC motor’s maximum rotation speed is limited only by the design of the motor; and electromagnetic interference, also known as EMI, is greatly reduced because there are no arching brushes. The only disadvantage of 3-phase brushless motors is the cost. This approach requires three half bridges instead of the two half bridges required for brushed DC motors. Normally, a more complex controller for controlling the brushless DC motor results in longer initial development time.

PTM פורסם ב: