Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
dc-motor-driver-slide9

In the following slides, the tutorial will be illustrating motor drive state examples. The colors of red, blue, and green represent three different coils with a common central node. The direction of current flow of the coils is shown for each of the six states of angular rotor position. For each angular position, the corresponding logic levels for the Hall sensors, HA, HB, and HC, are also color coded. The average applied voltage waveforms to each motor connection, MA, MB and MC, are also shown. A simplified 3-phase schematic also illustrates the state of the bridge FETs and the direction of current flow.

PTM פורסם ב: