Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
Slide4
A buck-boost converter is ostensibly just a combination of a buck controller and a boost controller. In buck mode, the transistor Q4 acts as a closed switch and Q3 acts as an open switch. Q1 and Q2 modulate based upon the required load. In boost mode, Q1 is in the closed position, Q2 is open, and Q3 and Q4 modulate depending upon the load. When VIN is close to the same value as the required VOUT, then the device may alternate between bucking and boosting the circuit as shown in the next slide.
PTM פורסם ב: