Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Product List
JWPF-Slide5

A seal ring is applied for complete sealing at the mating side which is located in either the header or in the tab housing depending on which series is being used. The seal protects the interface, when mated, from moisture, dirt, scratches and cracks. A solid rubber seal is used for wire side sealing that makes the size compact. The contact system has a double spring construction that ensures superior contact force.

PTM פורסם ב: