Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Product List
JWPF-Slide7

Contacts are “clean” and designed without exterior locking lances which tend to become distorted, depressed, tangled or damaged through handling. The locking feature for the JWPF series is internal to the housing. In addition to eliminating the concerns relative to the terminated wires, this design approach also assures the elimination of contact back out since the contact locking mechanism is fully within the connector housing.

PTM פורסם ב: