Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
LittelFuse 'SIDACtor' Devices

Next, this module will look at the effect of the applied voltage on the capacitance of the SIDACtor. The graph shown here is for a popular C rated 260V SIDACtor. With no voltage applied, the capacitance is quite high compared with the capacitance with just a few volts applied. Other SIDACtor devices will have higher or lower capacitance, but they all follow the same basic curve. In telephone voice circuits, this has no real effect. However, in data circuits this characteristic can cause data errors. This is why Littelfuse developed the MC line of SIDACtor devices. These devices have significantly less capacitance than the standard line and are ideal in applications such as T1/E1, ADSL and ISDN. For very high speed data circuits such as VDSL or Ethernet, Littelfuse recommends biased bridge technology devices. These are the SDP and SEP protectors and are specifically designed to eliminate this capacitance issue.

PTM פורסם ב: