Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
LittelFuse 'SIDACtor' Devices

Overvoltage protection devices can be divided into two classes. Clamping devices limit the voltage to a fixed level. In doing so, they absorb the excess energy of the overvoltage event as long as the event is present. TVS diodes are an example of clamping devices. Crowbar devices, once triggered, essentially short out the protected line, redirecting the excess energy away from the protected circuit. Once the overvoltage event has stopped, crowbar devices will “delatch” and allow the circuit to resume normal operation. Because they short out the protected line when activated, crowbar devices are used only in applications where the available power is limited such as telephone circuits, data lines and signaling systems. SIDACtor devices are all crowbar devices.

PTM פורסם ב: