Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
LittelFuse 'SIDACtor' Devices

VDRM is the maximum voltage that can be applied to the SIDACtor device without triggering the device into conduction. The threshold for conduction, called IDRM is usually defined as 5 microamps. This means that the VDRM value should be larger than the highest expected operating voltage of the system. If operating voltages exceed the VDRM, even for an instant, the SIDACtor device may interfere with the system operation.  Because increasing temperatures will increase device leakage, the VDRM will drop with increasing temperature.

PTM פורסם ב: