Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List

Spa-Slide13

The parameter VBR does describe a protection aspect of the TVS diode array. VBR is the breakdown voltage of the device. It is the voltage at which the array will begin to protect and conduct current. This voltage may be specified at a couple different test currents. Commonly the VBR is specified at 1mA.
 
PTM פורסם ב: