Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
Spa-Slide23

In summary, TVS diode arrays are most commonly used to protect against ESD. Most ICs have some type of built in ESD protection, unfortunately this ESD protection is only considering the manufacturing environment and not real-world applications. The IEC61000-4-2 standard addresses ESD events seen in the field or at the system level which involves much higher current. As most manufacturers will test to this specification, external ESD protection will be required. Littelfuse TVS diode arrays will aid the designer in protecting their devices beyond the manufacturing level.

PTM פורסם ב: