Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
Spa-Slide17

The RDYN is calculated by taking the difference of two clamping voltages generated by two different current levels and using the relationship of R equals V divided by I. As shown here, the two current levels are 1A and 2A so when the clamping voltage is subtracted at these two levels and divided by two minus one, or simply one, it makes the calculation very simple. This parameter is by far the best way to compare protection devices between different manufacturers.

PTM פורסם ב: