Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
Strengths

As with the other zero-drift amplifiers, the self-correcting architecture of the MCP6N16 provides superior DC performance, including low initial offset and low offset drift. In addition, the zero-drift architecture provides for excellent common mode and power supply rejection, which is important since INAs are commonly used to reject these unwanted signals.

PTM פורסם ב: