Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
Industrial
The first target market this presentation will focus on is instrumentation, sometimes referred to as data acquisition. Instrumentation covers a wide range of applications covering industrial, consumer, medical, and even automotive markets – anywhere that a sensor is monitoring a physical condition. Specific examples within industrial instrumentation are included here. A pressure sensor used to monitor a compressed natural gas fuel line may use an instrumentation amplifier. Fabricating integrated circuits is a good example of the need for factory or process control (closely monitoring temperature, pressure, chemical levels, etc.) Also, water or sewage treatment plants utilize sensors for monitoring/testing purposes. White goods also use instrumentation circuits to monitor various conditions, such as the vibration of an industrial washing machine, monitoring the water level, and temperature control.
PTM פורסם ב: