Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Product List
HDMITFT-Slide2

Throughout the years, High Definition Multimedia Interface (HDMI) has developed into a widely used interface and is becoming more in demand as technology continues to advance. A key contributor to the growth in popularity of HDMI is the standardized digital format. HDMI implements standards that define video formats, quality, and is evolving into an interface that can support optional advanced features such as 3D, Ethernet data, and Consumer Electronics Control extension. With the growth of electronic advancements, HDMI is becoming a quick replacement for analog video devices. Newhaven Display recognized the need for a simple and powerful interface to be incorporated into the display line and therefore created the HDMI TFT Module Displays. These TFT HDMI modules incorporate HDMI interface and are designed to work with any computer that has HDMI output. Now users can use the advancement of HDMI interface with high-performing TFT displays. In addition to the easy-to-use HDMI interface, Newhaven took this display line a step further and incorporated USB-Human Interface Device (HID) into the touch panel versions within the display line. USB-HID is a part of the USB specification for computer peripherals and specifies human interface devices that work with computers. This means that using the touch panel on these HDMI TFT modules is as simple as plugging in a computer mouse for the first time. As soon as the Micro USB cable is connected from the HDMI Module to the source with USB compatibility, drivers automatically download that enable the touch function on these displays. Newhaven Display’s HDMI TFT modules are truly the next step in advanced TFT development for Single Board Computers and Embedded Display applications.

PTM פורסם ב: