Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
Image of Octavo Systems Overview of the OSD32MP1 System-in-Package Family - OSD32MP1-BRK

The best way to get started is to get one of the development platforms from Octavo Systems. The first one is the OSD32MP1-BRK flexible prototyping platform. It is a small, low-cost platform the size of a business card. This board shows how easy it is to design with OSD32MP1 and what little hardware is needed to go from the SiP to a board booting Linux and working peripherals. It is a 4-layer board, with all of the components on a single side, yet it can provide access to almost all the pins of the MP1. The design is open source, providing all of the schematics and layout files.

PTM פורסם ב: