Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
Image of Octavo Systems Overview of the OSD32MP1 System-in-Package Family - Optimized BGA

In addition to the simplification of the actual design, the OSD32MP1 significantly simplifies the layout process through the design of the ball map on the system-in-package. A 302 ball BGA 1mm pitch gives access to all the I/O's that are on the MP1. Octavo Systems has arranged those I/O's in an intelligent manner that allows designers to access all of the I/O's on the outer three layers with power and ground pins all in the center.

PTM פורסם ב: