Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
Image of Octavo Systems Overview of the OSD32MP1 System-in-Package Family - Developing with OpenSTLinux Distribution

This workflow here shows the steps used to integrate the OSD32MP1-BRK into the OpenSTLinux distribution. Octavo Systems provides a set of patches for the TF-A, U-boot, and the Linux kernel. Once designers download these patches they then apply them to each component after they are downloaded. Once the patched components are built, copy those binaries into the starter package. That is all there is to it.

PTM פורסם ב: