Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
Semiconductor General Purpose 24 Volt Motor Drivers Slide 18

As can be seen on this slide, packages are unified across current ratings within a family of parts. They share the same foot print and pin out so that as current ratings change, and IC change is all that is needed, not a PCB change. The stepper motor drivers can also be used as two channel forward/reverse motor drivers.

PTM פורסם ב: