Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
Semiconductor General Purpose 24 Volt Motor Drivers Slide 3

Shown on this slide is a partial list of motor drivers and common applications in which can be seen the purpose of the motors in each application, the recommended products, and the motor type. The machines that handle money need motors for handling currency, access cards, and receipts. Games have motors to move drums and crane arms. Office equipment has time cards and print head control. The industrial market has many applications of motors such as the vending machines needed to move goods out to the consumer, and the textile industry deals with moving different types of materials.

PTM פורסם ב: