Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
rx dev
As with the rest of the RX family, RX651/RX65N is supported by a host of development and debugging tools. e2 studio is the free Renesas Integrated Development Environment (IDE) based on Eclipse. The RX651/RX65N is also supported by the industry standard IAR tool-chain. A number of debugger options including the Renesas E1, E20, E2 Lite, and Segger J-Link are all compatible with RX651/RX65N. Supported compilers include the Renesas RX compiler as well as the IAR compiler and open source GCC compiler.
PTM פורסם ב: