Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
Ambient Light Sensors Slide 17

The BH1700 family has two I2C slave addresses which gives the design engineer flexibility when designing an end-product. This feature is useful in an application requiring two digital light sensors, in which case, the designer can assign one I2C address to each light sensor. This would also be useful in applications that have a component with the same I2C address as the light sensor.

PTM פורסם ב: