Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List
app block dia
The data logger using the ML630Q466/Q464 requires minimal external components compared to conventional designs. Just add the required sensors or thermistors and power to use the device. If additional timing accuracy is needed, an external 32 kHz crystal can be added as well.
PTM פורסם ב: