Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
setting para for simulation
To help designers with using right values, ROHM offers simulation tools for these DC/DC Converters. Shown here is an example using the BD9E303EFJ. By inputting the parameters into the fields, the tool will calculate the rest of the circuit. The simulation also allows engineers to run steady state, load response, and efficiency curves to generate the graphs as shown on the next two slides.
PTM פורסם ב: