Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
surface-mount-slide5
The advantages of shielded vs. un-shielded inductors should be considered when making the initial selection. Shielded inductors present low magnetic radiation because a special protective shield is incorporated to their design. The magnetic field generated by the inductor is contained within the unit by virtue of this shield surrounding the entire frame. The powerful magnetic shield utilized in the shielded SMD series produces the value added benefits of yielding higher inductances and lower DC resistances per the same volumetric size as their un-shielded counterparts. For applications where EMI is posing a critical challenge, the shielded SMD power inductor is a dependable and highly reliable cost effective solution. Signal Transformer provides eighty different product series of  shielded SMD power inductors. The seven products shown on this slide represent some of the packaging options available.
PTM פורסם ב: