Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
surface-mount-slide6
Signal Transformer application engineers are often asked when a designer should specify a shielded inductor over an un-shielded one. Once current is applied to an inductor, a magnetic flux field is generated, radiating from the part, and can couple with adjacent components or circuitry. With a shielded power inductor, the majority of this magnetic flux is kept inside the package, safely confined. In an un-shielded power inductor the magnetic flux field radiates freely and may cause operational problems. Here are some other considerations: if un-shielded and shielded power inductors have the same inductance value in the same volumetric size, then the un-shielded structures would need more winding turns to achieve the same inductance value, so the DC resistance of their windings is higher.
PTM פורסם ב: