Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
mediagauge-slide13

A typical application is to use the MediaGauge™ MG-MD in a monitor and control system. In the example shown here, the MediaGauge MG-MD is attached to an external power supply, a current meter, and a relay. The MG-MD has user programmable high and low pressure set points. The 4-20mA output is proportional to the input pressure and operates independent of these low and high set points.

PTM פורסם ב: