Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
mediagauge-slide3

These mechanical dial gauges have a tendency to wear out prematurely from the stress of the movement, are messy when they leak the fluid used to dampen needle movement, and have an accuracy that is dependent on the operator. In addition, parallax error is common with analog gauges - the operator’s eye alignment with the needle during the reading can introduce more inaccuracies.

PTM פורסם ב: