Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
mediagauge-slide7

The MediaGauge digital pressure gauges use stainless steel diaphragms to media isolate the piezoresistive sensing element. The electrical output from the sensing element is proportional to the input pressure applied to the diaphragm. Signal conditioning circuitry inside the MediaGauge compensates for temperature and calibration. The end result is that the MediaGauge MG-9V and MG-MD models have a high accuracy of +/-0.25 % full scale independent of who reads the gauge.

PTM פורסם ב: