Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
Wireless Modules Slide 10

The power management for the SPWF01S module has very low power modes shown here with the current consumption in run mode. The current consumption in sleep mode or when the microcontroller is in stop mode is less than 1 mA of power consumption. The standby mode is where the radio and the microcontroller are both in standby mode, the current consumption is 5 µA.

PTM פורסם ב: