Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
Wireless Modules Slide 5

The key features, key factors, and the key benefits of this module are shown here. First of all the radio supports b, g, and n standard, so this allows an easy integration in every WLAN system. The module is fully integrated, thanks to the reduced development and the time to market because the customer does not have to integrate the stack or the CPA stack with the application, this is already done inside the device. The module integrates either an antenna or a U.FL connector, so it simplifies the RF design. There is no need of RF knowledge for the integration. The module comes with CE, FCC, and IC certification, so it reduce the certification cost of the target application. There is no need of a driver or external protocol stack in order to use the modules. The modules are very small. The Wi-Fi modules integrate TCP/IP and application layer functionalities. Very important, the temperature range is industrial, so this is basically perfect for any type of machine-to-machine application in the industrial environment or where the industrial temperature range is needed. The modules are also good for the mass market, being a fully-integrated solution.

PTM פורסם ב: