Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
Wireless Modules Slide 4

The SPWF01S Wi-Fi module is a serial-to-Wi-Fi module with a serial interface on one side that allows communication with microcontrollers like STM32 and STM8. On the other side, it is connected to the Internet with the Wi-Fi transceiver. The module features two chipsets, a microcontroller that takes care of the application utilities and the stack and a WiFi chipset, the CW1100. So the entire silicon solution on this module is an ST solution.

PTM פורסם ב: