Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Product List
H48 Product Range Slide 21

It is essential that the products are used within their correct design guidelines. All gap filling materials should be used under compression for optimum thermal performance. Ideally, this compression should be from 20 to 45%, based on the original thickness. This allows the product to wet the surface and form a good interface between the source and the sink. For use outside of the parameters stated in the datasheets, please contact T-Global directly.

PTM פורסם ב:
PTM Updated on: 2015-06-19