Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
TG-NSP35 Slide 16

In summary, t-Global’s TG-NSP35 is a one part, fully cured, non-silicone thermal putty with a thermal conductivity of 3.5 W/mk. This thermal conductivity will allow it to address most of the common thermal issues facing the automotive industry. It has been specifically designed for the automotive industry and passes all the common thermal, mechanical and environmental tests common to this market sector. TG-NSP35 offers an exceptionally low total cost of ownership approach for the automotive industry. As TG-NSP35 is a non-silicone product it will not out-gas and this is seen as a distinct advantage when compared to silicone products commonly used in the automotive industry.

PTM פורסם ב: