Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
Closed-Loop Hall Effect Sensors Slide 11

Frequency bandwidth or frequency response is another important feature of the closed loop Hall Effect sensor, and is an indication of the ability of the current sensor to accurately measure high frequency input signals with minimal loss in fidelity and attenuation. High frequency signals over 100kHz can be measured with less than 1dB of attenuation.

PTM פורסם ב: