Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
Closed-Loop Hall Effect Sensors Slide 4

The Hall Effect element is a 4 terminal semiconductor device typically fabricated from InAs material, which is selected for the material’s sensitivity to a magnetic field. The Control Current (IC) biases the Hall Effect element in a quiescent state. The incident magnetic flux creates a charge separation resulting in a potential difference represented by the Hall Voltage, VH. The VH is further signal conditioned and used to control the secondary current. The secondary current is driven through the secondary winding to generate the counter-flux needed to cancel the flux generated by the primary current.

PTM פורסם ב: